3/14/2023 2:41 PM | |
Joined: 3/30/2020 Last visit: 5/26/2024 Posts: 4537 Rating: (946) |
Look at the attached image. The ANY pointer description on the input is copied over onto temporary storage. Then it is used in the PUT instruction. You will have to test if it works though. As SCL reference you can have a look at: https://support.industry.siemens.com/forum/de/en/posts/data-type-any-in-scl/38978 |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to2 thankful Users |
Follow us on