3/30/2023 11:48 AM | |
Joined: 3/30/2020 Last visit: 5/25/2024 Posts: 4537 Rating: (946) |
Hello. My previous response had a idea which were meant to further discussion. But the idea was flawed and did not fulfill the requirement. The following design fulfill the requirement. The implementation would look like something in the picture below. It is assumed that DB10.DBX3.5 is the bit to be triggered for conveyor 1. Attached is the ZIP of the source code. Indirect addressing is used to influence all the bits associated with the conveyor manual override. The pointers can be changed to suit the changing situation but it is assumed that the each conveyor's trigger bit is 1 byte away for the next. ~ AttachmentTriggerConv.zip (224 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on