(0)| 4/7/2023 2:43 AM | |
|
Posts: 1 Rating:
|
I need to control 3 identical motors from a HMI. So I make one faceplate of the motor, and 3 buttons for valve 1, 2 and 3. Also I create 3 HMI tags, valve_select for the valve #, Close_cmd_from_fp, Open_cmd_from_fp. My plan is, when the OPEN/CLOSE button is clicked, it will trigger a VB Script, OPEN_CLOSE_GATE_VALVE. In this script, it will read the above 3 tags, send the command to PLC, and write a message to the text field of the HMI. But the Text is not updated after open/close on the faceplate. If the VB script is activated by a button, then it can work. It looks like a HMI tag change can not trigger a VB script. To test whether the HMI tags can receive the click from faceplate, i made two symbolic IO fields under the text. Each time i click the OPEN/CLOSE, they can show NOT PRESSED/PRESSED. This is implemented with a text -list. But the changes of the HMI tags Close_cmd_from_fp and Open_cmd_from_fp, can not activate the VB script. If the answer is No, an internal HMI tag can not trigger the VB Script, how can I solve this problem ? As i have two parameters, valve # and operation, to determine where to send the command. My system is TIA Portal V16, Simocode ES V16, WinCC Advanced V16. HMI is Comfort TP900. Thanks for your help !! Attachmentsiemens.pdf (301 Downloads) |
| 4/20/2023 9:33 AM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello JimmyHOU there is a safety mechanism implemented in WinCC Comfort/Advanced for triggering with internal Tags check out this FAQ: "Why is a script, which is configured to occur in the event of a "change in value" of an internal tag, not executed?" https://support.industry.siemens.com/cs/ww/en/view/57132412 If you would change the internal trigger in an IO field then it would work but not with Systemfunction or script change. Its a system behaviour and cannot be changed Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on