2/11/2016 4:07 PM | |
Joined: 4/28/2015 Last visit: 9/13/2024 Posts: 10 Rating: (0) |
Nice one thank you |
2/12/2016 7:12 AM | |
Posts: 2930 Rating: (432)
|
Hi, less effort: Time is mapped to VWx: Just writte into VWx from the HMI. In this case no need to use ANI and an analog amplifier with referenz. |
2/12/2016 2:11 PM | |
Joined: 4/28/2015 Last visit: 9/13/2024 Posts: 10 Rating: (0) |
Thank You |
4/25/2023 4:06 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by pynista is split to a separate thread with the subject What happens to the timer setting if the connection between HMI and Logo fails?. Best regards |
Follow us on