2/17/2023 7:36 AM | |
Joined: 7/10/2012 Last visit: 11/22/2023 Posts: 2 Rating:
|
Hello BGImmelman Thank you for sharing the solution , this is very helpful . i have a question about the dummy script did u create 1024 line in your dummy script ? dummy 1 = .....[1] ...dummy1=....[1024] i try this solution and i only can acces the element of the array that i mentionned in the dummy script thank you in advance |
5/5/2023 12:10 PM | |
Joined: 8/3/2009 Last visit: 8/8/2024 Posts: 13500 Rating:
|
Hello everyone This leads all to the definition that is explained in the TIA Help System: https://support.industry.siemens.com/cs/ww/en/view/109813306/109377913227 Check " Note Current system behavior for dynamic access to elements of a user data type... " so If you wnat to get access to the Tags in this dynamicc way they have to be used somewhere else that the data manager recognises them. so in case of the dummy script, every item has to be mentioned or you create a dummy screen where you drag and drop every element of the UDTs (this will only take a few seconds). You do not have to open this Screen in Runtime, it only has to be loaded. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on