5/18/2023 5:16 AM | |
Joined: 12/15/2016 Last visit: 9/21/2024 Posts: 61 Rating: (0) |
I have an IOT2040 FS: 01 01.2021 I have installed sample image v3.1.17 on it. and in the IOT it works correctly, so far so good. In nodered I want to install the telegram-contrib palette and it tells me that I can't because the version of nodered is low. I've tried everything, I install an older telegram-contrib palette, I get an error. I try updating NPM, with error, also updating Node also with error. Could someone tell me what solution I have to install the telegram-contrib palette. Thanks Edu Attachmenterrors.zip (333 Downloads) |
Follow us on