(0)| 5/26/2009 10:05 AM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Ab R; Direct Data Exchange is possible with Profibus drives, but at this time I am not able to locate the links for the Masterdrives. Here is a link to an application for MicroMasters, as a start it should give you some informationon the requirements for producer/consumer exchanges for Siemens drives: -you will require Drives ES to parameter the drive comm boards for this; -you will still require the presence of a Profibus master to enable the exchanges, even though the data does bnbot transit through the master. http://support.automation.siemens.com/WW/view/en/22421343 In any case, I have not done this personnaly, either with MicroMasters or Masterdrives, so this is all from research on the Support site. If anyone has more precise information, even contradictory one,I would welcome the opportunity, this is a very interesting question. Hope this helps, Daniel Chartier |
| 5/28/2009 3:15 PM | |
|
Posts: 3 Rating:
|
Thanks a lot for you answers. I believe I am stuck with buying a DP-CPU oranother optional communication board. Thanks again guys. |
Follow us on