11/2/2016 10:40 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello cnc_klemen, 828D is a panel-based CNC (panel processing unit). A CNC, PLC, operator panel and axis control for 6 drives (standard) are combined in one unit, it is medium performance in range. This design eliminates the hardware interface between CNC electronics & OP. If analog drive needs to be controlled, then 840Di SL with ADI4 configuration can serve the purpose. HTH. |
Last edited by: PISCEAN 2010 at: 11/2/2016 11:08:09 AM |
|
Follow us on