6/8/2023 1:19 PM | |
Joined: 9/27/2017 Last visit: 9/2/2025 Posts: 19 Rating:
|
Good morning, I am having a nightmare with the following error related to communication between 2 F-Runtimes: Temporary CPU error: User programmed STOP request in FB 2008 Checking FB2008 it is a protected compiler block named "F_PS_COMM_DEVICE" with the following description inside: F_: Protocol Driver Block Send PROFIsafe V2 + Protocolextension up to 100 Bytes Does anybody have an idea how to find the problem? Any help would be great. Thanks you all in advance |
Last edited by: Jen_Moderator at: 06/09/2023 09:52:48Link optimized. |
|
6/20/2023 7:32 AM | |
Joined: 9/27/2017 Last visit: 9/2/2025 Posts: 19 Rating:
|
More info. I have the following OBs: OB30: 5ms priority 16 F-RTG 1: 20ms priority 15 F-RTG 2 : 80ms priority 15 I was doing some test and looks like when I assign to F-RTG 1 and F-RTG 2 same priority as OB30 problem dissapear, but I can not do it as OB30 execution time get unstable. Do you think problem is produced by OB30 interruptions over F-RTGs? If somebody has any idea please let me know Best regards
|
Follow us on