6/13/2023 11:38 AM | |
Joined: 2/3/2022 Last visit: 4/23/2024 Posts: 304 Rating: (27) |
Hi! Maybe this is can be helpful. https://support.industry.siemens.com/cs/es/en/view/109760739/78806274699 Br! |
6/30/2023 8:43 AM | |
Joined: 2/16/2023 Last visit: 10/8/2024 Posts: 6 Rating: (0) |
Hi, I have attached the .PDL file I tried to copy between two different PCs. I am using WinCC Runtime V7.5 + SP2 / K7.5.2.0 while the other computer is running WinCC Runtime V7.4 + SP1 + Upd8 / K7.4.1.8. My PC is running a monitor with a resolution of 3840x2160 while the other one is a standard 1080p. Attachmentpopup_test.zip (220 Downloads) |
Follow us on