(0)| 6/22/2023 1:45 PM | |
|
Joined: 2/17/2020 Last visit: 1/22/2026 Posts: 1251 Rating:
|
Just found this information too, that applies to both WinCC V7 and WinCC Professional: "Using WinCC in multiple domainsThe correct functioning of WinCC can only be guaranteed when all the computers in a multi-user system are located in a common domain or working group. When WinCC is used in different domains or working groups, complications may arise if the access rights and/or name utility are configured incorrectly. When the user administration is realized in a working group, all the WinCC users must be set up on all the computers in the multi-user system and have the necessary access authorization.". Information on network technology and UPS You can find a similar description also here: "Note: Make sure that the domain server and domain client are in the same network, but have different IP addresses.". Installation and operation of WinCC in a Microsoft domain environment
|
|
A rating will be well appreciated. |
|
This contribution was helpful to
|
|
| 6/23/2023 12:59 PM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16661 Rating:
|
Hello Oscar_83PL If you cannot do an online download then you can also do a offline download with the download to filesystem function in TIA Portal.x https://support.industry.siemens.com/cs/ww/en/view/103198851 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 7/7/2023 12:50 PM | |
|
Joined: 10/22/2008 Last visit: 12/23/2025 Posts: 378 Rating:
|
Hi, I just wanted to save some time with the online download as it gives the option for delta downloads. As a workaround I used virtual machine.
|
Follow us on