7/14/2023 1:37 PM | |
Joined: 3/30/2020 Last visit: 9/2/2025 Posts: 5416 Rating:
|
The specifications for the IFM device is given From that the following extract: A 500ohm resistor is used to get a 10V signal, but..
As Mr. Jacek suggested - measure the voltage over the 500ohms and see if that relates to what the PLC gives. My opinions means nothing if the analog on the PLC does not correspond with the hand-meter's voltage measurement. Then there are some choices:
|
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
3 thankful Users |
Follow us on