6/3/2009 5:55 AM | |
Posts: 148 Rating: (11) |
you have to use the Profibus. |
6/3/2009 8:15 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Look at http://support.automation.siemens.com/WW/view/en/27864729
I guess this is new device and with BOP itsn't be possible to put IP address. Anyway: PROFINET IP address: see P08831 PROFINET IP subnetmask: see P08832 Hope this will helps. Best regards Hristo Mihalev |
6/3/2009 8:48 AM | |
Posts: 139 Rating: (25) |
Primary Setup Tool download http://support.automation.siemens.com/WW/view/en/19440762 |
Follow us on