8/3/2023 9:16 PM | |
Joined: 10/4/2016 Last visit: 3/25/2024 Posts: 3 Rating: (0) |
hello everyone I encounter this error when |
8/3/2023 11:48 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665)
|
Hello ahani; It appears that the programmer who created the project you are trying to open used a software for electromechanical design, linked to the PLC program, possibly this one, Simcenter: https://plm.sw.siemens.com/en-US/simcenter/simulation-test/electrical-system-simulation/ If you can use the original PC that has Simcenter installed, you can work with the original project. One option, if you cannot access the original PC would be to install Simcenter on your work PC. There is a trial (free download, time-limited to 60 days) version of all mechanical simulation software suite from Siemens PLM in the following link: If you want to remove the simulation software blocks from your Step 7 installatoon, I can only suggest you contact a Siemens tech through a Support Request, and inquire if you can somehow remove all blocks created through Simcenter from the program, so you can work with only Step 7. The link for a Support Request is located at the top of this page. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/04/2023 00:11:55 |
|
This contribution was helpful to1 thankful Users |
Follow us on