8/21/2023 2:36 AM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32895 Rating: (4067) |
The Hotfix 10 for STEP 7 V5.6 SP2 is available for download. Download Hotfix 10 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SRIn order to ensure high security standards, an archive consistency assurance is introduced. The following messages are relevant: Help on Message 3020:79Description of Error:Modified archive files were found. Possible causes:·The data have been changed by another user in the project or by the transfer of the data. ·The project archive was created secure with the current STEP 7 version. The project was then edited and archived again with an older STEP 7 version. Only retrieve the project, if you can exclude through further IT security measures that the data has been manipulated with non-STEP 7 tools. To Correct or Avoid Error:Check the project consistency and, if necessary create a new archive. Help on Message 3020:81Description of Error:No information about ensuring archive consistency was found in this project archive. Possible causes:·The archive was created with an older STEP 7 version. ·The archive was deliberately created without security information. ·The archive was created with another tool without STEP 7. ·The security information was removed from the archive using third-party tools. Note: If the archive does not contain information to ensure archive consistency, you must ensure it in another way. To Correct or Avoid Error:Check the project consistency and, if necessary create a new archive with the "Secure archive" option. Password Protection when Inserting a CPU |
This contribution was helpful to2 thankful Users |
Follow us on