8/23/2023 12:31 AM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
Sales Release and Download for Firmware 3.4.29 for CP 1242-7 V2, CP 1243-7, CP 1243-1, CP 1243-8Firmware version 3.4.29 for the following S7-1200 communication modules is available for download DESCRIPTION: Firmware version 3.4.29 for the following S7-1200 communication modules is available for download:
The firmware contains general product quality improvements and is used to upgrade devices of the above-mentioned products that are already in use. In particular, the firmware contains the following changes: Feature Enhancements:
Bugfixes:
Security fixes:
To configure the modules with firmware 3.4, TIA Portal Step7 V18 Update 2 (or later) must be used. The firmware is only compatible with devices of the above products that have hardware version 2 or newer. |
This contribution was helpful to
2 thankful Users |
Follow us on