8/24/2023 11:29 AM | |
Joined: 8/29/2022 Last visit: 11/3/2023 Posts: 23 Rating: (0)
|
Normally, it is possible to add Edge Device specific configurations in the following types, templates or file uploads. a) In case of *.txt based configuration files, the configuration file supports the configuration for Edge Devices with allocated tags. Any key that you add to the template-based configuration file in the format ""##$<KEY>$##" is replaced by its value that you have allocated to the Edge Devices through the created tags. To add them you should:
b) App configurations that base on *.json template files are used to configure and install the app via the IE Application Configuration Service (IE ACS). For more information:
Notice: Best regards, |
Follow us on