8/25/2023 8:19 AM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello Hanashima If you use Tags directly on the trend then only one tag can work with one trend, you cannot use one trend with the values of different tags. The only way to to this would be to change the Trend provider to none and write the values for the trends with VB Script and an Array. Here are some examples how you would do this: https://support.industry.siemens.com/cs/ww/en/view/109818193/45950651019 But this are only some basic examples but it shows how to provide any data to a trend in Function Trend control by Script. before you have to read out your Tag values Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on