12/10/2021 11:32 AM | |
Joined: 5/16/2017 Last visit: 4/17/2024 Posts: 3 Rating: (0) |
Attached error messages. |
12/10/2021 1:43 PM | |
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Hi jerguin, this should also be possible with V5.5 as far is i know. But if it works with V5.6 with the same exact hardware...there are indeed some version dependencies. Maybe there is also an update for V5.5 available which can help. In this FAQ, version dependencies are shown: What should you check when the F destination addresses cannot be assigned?"you need at least
regards sancruz |
Feedback appreciated, please rate |
|
9/2/2023 7:07 PM | |
Joined: 4/19/2023 Last visit: 3/3/2024 Posts: 1 Rating: (0) |
How can I open this ?? I canot find this |
Follow us on