(0)| 9/12/2023 9:52 AM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi TimoRamone, Starting with FW 2.8, TIA Portal V16 is used as you can see in the following link: Therefore, it would be advisable to use the TIA Portal V16 to work with that CPU since you have it, I understand. From what I see, it only works with V14, what problem exactly do you have with V16? You can work in V14 as you are doing but simply selecting version 2.1 is not possible with higher versions. The only thing that limits you are the possible updates that the new PLC firmwares have, nothing more. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
Follow us on