9/20/2023 8:42 AM | |
Joined: 7/26/2022 Last visit: 4/16/2025 Posts: 6 Rating:
|
Wait, is this TIA Portal? If it is, where did you get dark theme? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/20/2023 12:47:48New subject after splitting |
|
9/20/2023 2:08 PM | |
Joined: 7/19/2022 Last visit: 9/2/2025 Posts: 436 Rating:
|
I think that it isn´t TIA Portal |
If this Information really helps, you could use the Rate function |
|
9/20/2023 2:24 PM | |
Joined: 3/30/2020 Last visit: 9/3/2025 Posts: 5421 Rating:
|
You are correct. (TRIVIA) The segment shown in the original post (see below) is from a text editor with a "One Dark" colour theme. The theme was popular in the Github Atom text editor.
The colour theme is also available in Microsoft's Visual Studio Code (link). The code highlighting can be done in VS Code by using an add-on (link). |
Last edited by: qwazee at: 09/20/2023 14:25:46Use of the linked software modules are at own risk. Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
3 thankful Users |
Follow us on