9/1/2023 12:13 PM | |
Joined: 5/30/2014 Last visit: 6/27/2024 Posts: 146 Rating: (18) |
Hello, I have a similar problem with the same ADFweb device (HD67719-IP-A1), but in other direction. On BACnet side (PXC001-E.D) I read values (around 160 values, no values written from BACnet) sent from the S7-300 (programmed in Simatic Manager) and most of the time they are zeroes (from time to time it appears the right value for a moment). I checked ADFweb also with S7-1200 (programmed with TIA v16) and it seemed to work good. However, it was a static test (different values in different variables, but not changing in time) and when I attached S7-300 which have real values (sensors etc.) which change very quickly, it doesn't work. I tried to map only few values (around 5) and then it works. However, with more than 20 it collapses. I suspect that error is in ADFweb device and I need to know is there any possibility that problem is on Simatic side. Had someone experience with this device working? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/25/2023 07:02:18New subject after splitting If you find my contribution helpful please RATE it :)) |
|
Follow us on