(0)| 10/13/2023 8:03 PM | |
|
Joined: 9/21/2020 Last visit: 1/11/2026 Posts: 5 Rating:
|
I have an issue where the project upgrade fails, it creates a log file that I have added here, but I am not familiar with reading the log file. Is there anyone who can help put me in the right direction to solve the project upgrade issue? There is a line in the file that say: FS Server error: Reorganization failed in IntegrateFilePhase! RootCause: ReintegrationResult: Failed! Reason: It could not exchange the files, ErrorDetail: StorageController.Exchange: IOException occured: System.IO.IOException: Kan ikke opprette en fil når filen allerede finnes. The last sentence translates to: can't create a file when it already exists. AttachmentConversionLog_17.0.0.0_to_18.0.1.0.txt (347 Downloads) |
Last edited by: GeirN at: 10/13/2023 20:06:18 |
|
| 10/14/2023 6:25 AM | |
|
Joined: 9/21/2020 Last visit: 1/11/2026 Posts: 5 Rating:
|
I ran a basic integrity check from the project menu in V17, and then after upgrading it to V18, it worked. |
Follow us on