(0)| 10/23/2023 6:50 PM | |
|
Joined: 1/21/2013 Last visit: 1/19/2026 Posts: 4414 Rating:
|
Hi stefanigno, The use of L DINO requires the number of an instance data block available in the DI register. However, all of these operations are only possible when using standard block access. I am sure that your requirements can be met with optimized programming, but it will require a rethinking of your approaches. If you can describe your requirements in an accurate and understandable way, we volunteers may be able to help you get on the right track. Kind regards |
| 10/24/2023 7:47 AM | |
|
Joined: 1/21/2013 Last visit: 1/19/2026 Posts: 4414 Rating:
|
Hi stefanigno, The reason why you can't access the data block register is that the CPU doesn't have such registers. The registers are only emulated by the CPU. Please refer to "Data Exchange in STL" for more details. For us volunteers it is impossible to give some programming hints to meet your requirements without knowing them. Kind regards |
| 10/25/2023 9:15 AM | |
|
Joined: 10/25/2016 Last visit: 1/8/2026 Posts: 54 Rating:
|
Yes the db[dbnum] is in the hmi side |
Follow us on