(0)| 12/1/2023 9:30 AM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, It is not permitted or it does not work if the old module is installed but a newer one is configured. The modul 6ES7 151-1AA02-0AB0 had his product cacellation 2003, so it´t not contained in TIA. So try to project it with GSD. PROFIBUS GSD files: ET 200SRegards, Towome |
|
|
|
This contribution was helpful to
|
|
| 12/8/2023 6:55 PM | |
|
Posts: 2 Rating:
|
Hello Towome, I projected it as you suggested, and have used the old catalog gsd files for 6ES7 132-4HB00-0AB0 a 2DO module. It appears that each card is occupying 1 byte each of the Q address. It will not let me pack the addresses. Is there anyway to pack these addresses? If I address a bit outside of x.0 or x.1 will this use the next card? Its almost like TIA Portal sees it as a peripheral.
|
Follow us on