12/15/2023 8:01 PM | |
Joined: 6/8/2023 Last visit: 3/4/2024 Posts: 4 Rating: (0) |
Hello everyone: I have a problem with a proxy device, when I want to update I cannot see the device in the available box and the update fails. I share how my network is integrated and the proxy device that I want to update is Press_2. I have previously made updates, in this case Press_1 is updated without problem. Could someone suggest a solution to me, this was because I need to make some modifications to the HMI.I appreciate it, Regards I share images. ------------------------------------------------------------------------------------------ |
Last edited by: Daved23 at: 12/15/2023 20:03:16Last edited by: Jen_Moderator at: 12/18/2023 10:10:17New subject after splitting |
|
12/16/2023 7:42 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
and the error log? |
Follow us on