12/21/2023 7:03 AM | |
Joined: 1/3/2022 Last visit: 1/6/2024 Posts: 6 Rating: (0) |
Hi everyone, I have the conversion on S595U PLC to S71200 PLC. I already completed 80% of work and the process is not running as same as before finally i found the block OB251 in S5PLC. i can't open this block in S5 and i understand this is the own PID block for S5 PLC .so my support is i need to the conversion in the S71200 plc . can you please anyone give any hint to do that .the below program they used OB251. PLEASE SUPPORT L KF +0 T FW 200 A I 72.2 O I 72.3 = F 201.0 A( O I 72.0 O I 72.1 ) AN F 101.7 = F 210.0 A F 210.0 S F 101.7 AN I 72.0 AN I 72.1 R F 101.7 AN F 210.0 A F 100.0 AN I 72.2 AN I 72.3 = F 201.0 AN F 201.0 = F 202.2 L FW 200 T DW 11 L DW 53 T DW 9 L DW 54 T DW 22 AN I 72.2 AN I 72.3 L KF +0 JC =M001 L DW 63 A I 72.3 JC =M001 CSW M001: T DW 12 JU OB 251 L DW 9 L DW 22 -F T DW 56 BE ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2023 08:53:44New subject after splitting |
|
12/21/2023 8:54 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Conversation of PID block for S5 PLC to S7-1200 is published within the conference SIMATIC S5 / STEP 5. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on