1/2/2024 8:56 AM | |
Joined: 12/4/2015 Last visit: 4/3/2024 Posts: 15 Rating: (0) |
Hello again , sorry for delay. No .im an engineer working with cnc tool machines. This machine is quaizer mv204ii. 810d controller with ccu1 Pcu 50 4 axes . The problem is thatafter any power off/on We must set the manufact password and then set the some parameters for enabling the 4th axis(1a axis). "axis md:30130 Axis md:30240 Drive config: axis 4 active" In the attachement.you can see them . Before power off if i set these parametrs.there is no problem. i think that if the password remains when the device is turned off and on, the 4th axis may remain active. Best regards. AttachmentDownloads.zip (161 Downloads) |
Last edited by: Jen_Moderator at: 01/02/2024 11:25:21Text formatting optimized. |
|
1/6/2024 4:11 AM | |
Joined: 12/4/2015 Last visit: 4/3/2024 Posts: 15 Rating: (0) |
Hello again , sorry for delay. No .im an engineer working with cnc tool machines. This machine is quaizer mv204ii. 810d controller with ccu1 Pcu 50 4 axes . The problem is thatafter any power off/on We must set the manufact password and then set the some parameters for enabling the 4th axis(1a axis). "axis md:30130 Axis md:30240 Drive config: axis 4 active" In the attachement.you can see them . Before power off if i set these parametrs.there is no problem. i think that if the password remains when the device is turned off and on, the 4th axis may remain active. Best regards.
AttachmentDownloads.zip (148 Downloads) |
Follow us on