(1)| 1/22/2024 1:02 PM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Which HMI device/System do you use? In WinCC comfort/Advanced, I would say this is not possible because the name of the alarm log is a fixed setting in the engineering projekt. you can do a copy of the alarm log and rename it but this will only be a copy and not the running archive file: https://support.industry.siemens.com/cs/ww/en/view/63042926 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on