1/31/2024 11:52 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating:
|
Hi! Are you using WinCC Advanced or Professional? If you are using the lastly, you should implement a Server-Client architecture, as it is explained here: Plant Configuration Using WinCC Runtime Professional |
If this post helped you in any way, please rate it positively. |
|
2/6/2024 9:28 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16461 Rating:
|
Hello Khanaamir78624 Yes without more information we cannot give an exact suggestion. But you can can access the same PLc and DBs with more than one HMI parallel.Check out this FAQ for general information: https://support.industry.siemens.com/cs/ww/en/view/109479986 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on