2/11/2024 7:02 AM | |
Joined: 8/5/2023 Last visit: 10/7/2024 Posts: 14 Rating: (0) |
Hello Sir, I can't find good answer about my question |
2/11/2024 9:41 AM | |
Joined: 3/30/2020 Last visit: 10/20/2024 Posts: 4885 Rating: (996)
|
You are not suppose to be able to make a backup form a PLC that is properly password protected. It would be possible to make copies of a PLC without consent of the designer if there was a way.
Contact Siemens support if the response from volunteers on this forum does not meet your needs. Use the "Support Request" link. Before doing so, study the chapter in the System Manual about the usage of the external memory card (LINK). Knowing this chapter will help you focus the conversation. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
2/11/2024 10:34 AM | |
Joined: 8/5/2023 Last visit: 10/7/2024 Posts: 14 Rating: (0) |
Ok thanks for your guidance |
Follow us on