(0)| 2/12/2024 6:07 AM | |
|
Joined: 1/21/2013 Last visit: 1/21/2026 Posts: 4423 Rating:
|
Hi Roby, Knowing only a portion of the diagnostic buffer without other details, such as the PLC firmware version, makes it difficult to provide a proper response. What the screenshot shows is that the CPU goes into DEFECTIVE mode. The system code shown can be caused by several conditions, corrections have been made with the firmware versions: V2.8.3, V2.6.0 and V2.1.0. So it might help to do what the message says and install the latest firmware. Kind regards |
This contribution was helpful to
|
|
Follow us on