5/4/2023 10:27 PM | |
Joined: 4/6/2021 Last visit: 7/21/2023 Posts: 2 Rating: (0) |
Thanks for the post. Any idea of how to do it for Windows Server 2019, 64bit? I have modified the .ini files mentioned. Not sure what to write in the \InstData\Setups.ini. I have added the text mentioned. I have also tried with "Win2019=1" and "Win2019x64=1". Not working for the moment :( ------------------------------------------------------------------------------------------ |
Last edited by: juan_fernandez_uy at: 05/04/2023 22:28:30Last edited by: Jen_Moderator at: 05/05/2023 10:24:18New subject after splitting |
|
5/5/2023 11:10 AM | |
Joined: 2/17/2020 Last visit: 4/30/2024 Posts: 994 Rating: (169) |
Hi Juan, I have attached the WinCC Flexible 2008 compatibility list to the mail. As you can see, Windows Server is not among the released/tested operating systems. The problem with this is not just the installation (which is not working either), but the software can respond unpredictably after installation (closing unexpectedly, for example). My recommendation is that you use a released OS or otherwise virtualize the software within the Windows Server. AttachmentWinCC-flexible_2008_compatibility-list_en_2023-02-09.zip (543 Downloads) |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
Follow us on