2/27/2024 10:18 AM | |
Joined: 4/24/2008 Last visit: 4/18/2024 Posts: 206 Rating: (16) |
The size and shape of the updated configuration means that the new power modules are not spare parts compatible with the existing power modules. This should be considered during installation in the control cabinet. However they are hardware-compatible with the SINAMICS G120 CU2xx-2 control units, and for replacement purposes only the power module has to be exchanged. Maybe this product note help. https://support.industry.siemens.com/cs/ww/de/view/109743213/en |
Last edited by: The Helping Hand at: 02/28/2024 09:54:41Link optimized |
|
Follow us on