3/18/2024 10:01 AM | |
Joined: 1/21/2013 Last visit: 9/17/2025 Posts: 4110 Rating:
|
Hi, As the message indicates, WinCC Unified Comfort is optional. It depends on the devices in the project whether you need WinCC Unified or not. WinCC Comfort is fully covered by the installed WinCC Advanced and therefore you do not need to worry about it. If you have a WinCC Unified device in the project, you should install WinCC Unified. Even if it is part of the TIA Portal V17 STEP 7 / WinCC installation medium, it will not be installed by default if the required Windows features are not installed, which is probably not the case. However, as the message indicates, you must install SINAMICS Startdrive V17 to open the project. Kind regards |
3/18/2024 10:01 AM | |
Joined: 5/12/2006 Last visit: 9/16/2025 Posts: 22710 Rating:
|
start TIA V17 Help ->installed SW expand all packages and upload a screen of this |
3/18/2024 10:07 AM | |
Joined: 1/21/2013 Last visit: 9/17/2025 Posts: 4110 Rating:
|
Hi, You cannot install WinCC Unified if the required Windows features are not installed, which is not the case on a standard Windows system. Therefore, you must first install these features and then repeat the setup. Kind regards |
3/18/2024 10:29 AM | |
Joined: 3/2/2020 Last visit: 10/3/2024 Posts: 14 Rating:
|
Attached is the software list for both V16 and V17 as this is a V17 project showing a V16 HMI. |
Follow us on