(0)| 4/24/2024 9:02 PM | |
|
Joined: 3/26/2019 Last visit: 11/17/2025 Posts: 4 Rating:
|
Hello, We have a project fitted with 4 screens (1 TP1200 & 3 TP700). The alarms are allright on the TP1200, but on the TP700 we have the following problem: In the Hmi alarm configuration screen, the trigger bit is ok for the TP1200, but it's in error (pink) on the TP700. The PLC tags in use are the same on both screens, so the tigger bits are the sames. (You will find printscreen of the problem in the pdf attached to the message). I can't understand this behaviour. (same behaviour on TIA V14.1 & TIA V17) I hope someone here is more experienced than me Thanks for help. AttachmentTia_Alarms.pdf (295 Downloads) |
Last edited by: maint42 at: 04/24/2024 21:02:52Last edited by: maint42 at: 04/24/2024 21:14:27 |
|
Follow us on