5/4/2024 7:39 PM | |
Joined: 4/10/2024 Last visit: 5/5/2024 Posts: 3 Rating: (0) |
Does anybody have solution for this issue because i am also facing same issue..Motor low rpm issue is detecting..I am suspecting its the issue from process side and some thing is restricting the moment of motor shaft. in our case normally motor will run at 2800 rpm but after production started few hours hmi triggering alarm of low rpm but vfd doesn't have any fault..we are using 2.2 kw siemens motor with sinamics G120 VFD..please help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/06/2024 09:32:52New subject after splitting |
|
5/6/2024 9:33 AM | |
Joined: 6/19/2017 Last visit: 6/3/2024 Posts: 8123 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Sinamics G120 drive motor low rpm issue is published within the conference SINAMICS G. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on