6/12/2024 2:52 PM | |
Joined: 7/25/2012 Last visit: 6/12/2024 Posts: 259 Rating: (77) |
Hello, latest FW version for ABT Site V5.1 is signed_FW_V8.0_DXR2_V01.21.172.22-6095.fmwz It is part of the library 51_07 - it can be downloaded from : https://support.industry.siemens.com/cs/ww/en/view/109780759 But check you system version on DXR2 device - in property pane - system. It should be V8.0. If not, then I would like to recommend to update to latest version via : Application overview - button "Check update" - then select template and update. |
Last edited by: The Helping Hand at: 06/13/2024 08:23:58Link optimized Best regards, |
|
Follow us on