5/21/2024 1:19 PM | |
Joined: 4/18/2021 Last visit: 8/11/2024 Posts: 10 Rating: (0) |
I'm reaching out to seek assistance with a technical issue I'm experiencing with ISTA WATER METER MBUS MODULE. 1. The reading shown on the water meter and the reading shown in the software are not the same. But still am getting some data nearby on mbsheet and its increasing linearly. 2. A few hours after software integration of the water meter loses its communication, the energy meters of another manufacturer connected in the same loop are working properly. There are 6 to 8 water meters and 3 to 4 energy meters are connected in one loop, similarly 3 loops will connect in to one Mbus to RS 485 converter.
we've tried the following steps 1. Less number of water meters in one loop. 2. Water meters are connected as stand alone by removing the energy meters from loop 3. Connecting all devices in the loop by avoiding star connection. Unfortunately, the issue persists. The software we use for scanning and integration are 1. MB Sheet. 2. Siemens Xworks Plus. Attachmentwater meter 2.pdf (121 Downloads) |
Follow us on