6/27/2024 7:01 AM | |
Joined: 6/15/2023 Last visit: 8/2/2024 Posts: 2 Rating: (0) |
Dear All, I having a S7 1200 1215 CPU there are 2 Modbus TCP devices configured in inbuild ethernet port of CPU and I wanted to add one communication module for specific Modbus TCP communication. So please specify which module is to add for MODBUS TCP configuration. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/27/2024 11:22:23New subject after splitting |
|
7/3/2024 9:29 AM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating: (1713) |
Hello Rahul1 I´m not 100% sure but I would say CP1243-1 should work. Check also this opic: https://support.industry.siemens.com/forum/de/en/posts/cp-1243-1-as-modbus-server/244613 Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/4/2024 4:15 AM | |
Joined: 6/15/2023 Last visit: 8/2/2024 Posts: 2 Rating: (0) |
Thanks for a reply. That module works for Modbus Tcp protocol. |
Follow us on