6/27/2024 2:32 PM | |
Joined: 9/27/2006 Last visit: 7/17/2024 Posts: 12268 Rating: (2676)
|
Hello Ahmad; The Simovert Masterdrives are an older generation of drives, now replaced by the Sinamics family of drives. To select the appropriate gsd file for Profibus-DP for a Masterdrive, you have to know which communication board is inserted inside your drive, for example CBP2, CB1 I suggest you open the drive and look for the Profibus card (it has a sub-D 9-pin connector for linking to a Profibus network; a CBP2 has the part number 6SE7090-0XX84-0FF5, for example. Once you have determined the correct communication board, open this link and select the appropriate gsd file for your drive: https://support.industry.siemens.com/cs/ca/en/view/48172137 Hope this helps, |
This contribution was helpful to1 thankful Users |
7/1/2024 1:17 AM | |
Joined: 9/27/2006 Last visit: 7/17/2024 Posts: 12268 Rating: (2676) |
Hello Ahmad; Based on this document, the Simoreg 6RA70 also uses a CBP2 as a Profibus interface, and therefore would need a gsd file designed for the CBP2. Open the following link, download the masterdrive_cbp2.zip file; when you extract the files, look for the s9028045.gse file (for the English version), which you can integrate to your programming software, and also open with Notepad if you want to read the contents. https://support.industry.siemens.com/cs/ca/en/view/109474928 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on