9/27/2023 7:16 AM | |
Joined: 2/12/2008 Last visit: 8/2/2024 Posts: 70 Rating: (0) |
Hello, did you solved with this problem? Since this week I have the same issue, but it happen on two differen virtual machine, one is TIA17 and the other is TIA 15.1 both based on Windows10. I think the problem is on the real machine which is a Windows 11, beacause running the Virtual machine on an other PC with Windows 10 I have no problems! Thankyou ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 10:36:45New subject after splitting. Quote inserted. |
|
7/3/2024 11:31 AM | |
Joined: 4/22/2024 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Did you solve the problem? I have the same problem. Every time I close a tab in simotion scout or close simotion scout, I get this error "failed to connect link may be broken"
|
7/4/2024 10:02 AM | |
Joined: 4/22/2024 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
I created support request. thank you for your advice |
Follow us on