5/11/2024 10:20 AM | |
Joined: 4/27/2024 Last visit: 9/7/2024 Posts: 1 Rating:
|
Hi everyone, I'm having a problem where WinCC tag management can't connect to the CPU. On the connection there is a question mark and it shows "Connection status: Unknown". My setup is composed by a PC running Windows 10 Pro 22H2 and a CPU 1513-1-PN (firmware V2.9) both connected to an ethernet switch. Both devices are in the same subnet 192.168.1.xx. I have already installed simatic NET and checked my PG/PC interface. From this PC, using TIA Portal V18, I can download and go online with this CPU so I assume the PG-PC configuration is good. In TIA I have checked "Permit access with PUT/GET communication from remote partner" and unchecked "Only allow secure PG/PC and HMI communication". I attached a PDF with some screenshots of my configuration. If someone has any suggestion and can help me I would really appeciate. Thanks AttachmentScreenshots.pdf (146 Downloads) |
Last edited by: Jen_Moderator at: 05/13/2024 09:16:06Text formatting optimized. |
|
7/1/2024 4:10 PM | |
Joined: 6/15/2024 Last visit: 7/18/2024 Posts: 1 Rating:
|
I am also facing same problem. have you found any solution ? |
7/4/2024 11:08 AM | |
Joined: 8/3/2009 Last visit: 9/11/2024 Posts: 13647 Rating:
|
Hello if you have WinCC V7/8 then check out this FAQs (If not then please give us more information about your used Versions): https://support.industry.siemens.com/cs/de/en/view/109798498 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on