4/23/2024 12:42 PM | |
Joined: 1/21/2013 Last visit: 8/27/2024 Posts: 3057 Rating:
|
Hi fk36, The next question you should answer for yourself is whether the printer prints the expected label when you enter a constant real value in your data block. Test this first without using the "S_CONV" instruction. If it works, check that S_CONV produces the correct output to print the label. I would expect this not to be the case as it is a very simple instruction. You may have better luck with the "VAL_STRG" instruction. If you have already figured out what the data in the data block should look like, please provide a few examples (with the actual value and the expected output). Please also pay attention to the consistency of the data. Since TSEND_C works asynchronously over several PLC cycles, you must ensure that the data does not change during this time. However, your current programming of S_CONV does not take this into account. Kind regards |
This contribution was helpful to
1 thankful Users |
4/28/2024 1:58 PM | |
Joined: 8/7/2022 Last visit: 7/21/2024 Posts: 11 Rating:
|
Hello @admin ,@Stefan Please give me support ,i have to solve that problem anymore .Please help me ! Regards |
7/21/2024 3:11 PM | |
Joined: 8/7/2022 Last visit: 7/21/2024 Posts: 11 Rating:
|
Dear Sancruz , What do you mean empy charachter .Could you explain it please . Thank you . |
Follow us on