8/8/2024 11:35 PM | |
Joined: 6/4/2008 Last visit: 10/4/2024 Posts: 1497 Rating: (324)
|
Hi SimonT, There is a facility to allow the drive to be made operable for a period of 500 hours Change the following parameters: U977.1= 0727 U977.2 = 0101 You may need to power cycle the drive after this. After the drive is operating, I would raise a support request ticket and enquire how to proceed. https://support.industry.siemens.com/my/ww/en/requests#createRequest You will need to provide the following parameter values to the representative in order that they can provide you with a suitable pin U976.01 = ? U976.02 = ? Regards, Graeme |
This contribution was helpful to1 thankful Users |
8/15/2024 6:02 AM | |
Joined: 2/12/2015 Last visit: 9/30/2024 Posts: 3 Rating: (0) |
Hi! Official answer from Siemens we got is that there is no way to get the F01 option activated. With best regards, SimonT. |
Follow us on