(0)| 9/13/2024 1:08 PM | |
|
Posts: 2 Rating:
|
The Bluescreen is: Stillstandcode: SYSTEM_THREAD_EXCEPTION_NOT_HANDLED Errorsource: ndis.sys |
| 9/13/2024 1:22 PM | |
|
Joined: 12/18/2014 Last visit: 1/20/2026 Posts: 36494 Rating:
|
Start a Support Request. |
This contribution was helpful to
|
|
| 9/18/2024 12:41 PM | |
|
Joined: 5/22/2020 Last visit: 11/25/2025 Posts: 56 Rating:
|
Hi, It looks like there is a problem with the netwerk drivers see: ndis-drivers try to update the network driver. |
|
|
|
| 10/24/2024 12:16 PM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, as far as I can remember, there was an issue which would cause this if the base version V17 was installed. It was fixed with a update for v17. So check if V17 without any updates was installed. If yes, install the latest updates. Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17regards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on