11/13/2024 7:27 AM | |
Joined: 7/9/2015 Last visit: 8/29/2025 Posts: 4443 Rating:
|
Hi, there is also a good FAQ for scaling - it´s for TIA but there are some good information, which could help you for scaling. How do you standardize and destandardize analog values with STEP 7 (TIA Portal)?Regards, Towome |
|
|
11/13/2024 8:34 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 5443 Rating:
|
Hello. You are using the S7-200 programmed with Step7 Microwin. It is important that you mention that and not leave it for volunteers to guess. The S7-200 works a bit different than other Siemens PLCs. Also note that there is an "S7-200 Smart" which is also not exactly the same. Best to also not write your query as if it is a phone text message (DM). Details are missed there. But thank you for putting down a screen capture. You have M-memory and V-memory to work with. There is much less M-memory. M0.0 is a bit that is in MB0 but also MW0 and MD0. The B W and D indicates the sizing but it overlaps so that MD0 contains M0.0 to M3.7 / MB0 to MB3 and so on. It is worth your time studying the manual: [S7-200 System Manual]. The memory concept is explained there. Then when it comes to scaling - best to review the specifications for the signal card as given in the manual (linked above). Also review a more product specific link: [How can you scale analog values with S7-200 in conjunction with CPU224XP and expansion modules EM 231, EM 232 and EM 235?]. Are these notes of help to you? [ EDIT ] Assuming you have a cooling fan driven by the motor. The fan cannot run if the target temperature is higher than the measured temperature. The fan do run if the target temperature is lower than the measured one. How much difference may determine if the fan runs slow / medium / fast (x3 outputs). You need to decide the method of control. PID / Fuzzy logic / Rule based / Model predictive .. |
Last edited by: qwazee at: 11/13/2024 08:41:21Last edited by: qwazee at: 11/13/2024 08:43:08Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on