(0)| 11/29/2024 10:14 AM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi Sc9667, Can you provide a screenshot if possible of the Multilingual Support in the PLC properties? If not, please can you specify if there are any languages that are selected to be downloaded to the PLC, and if there are, what project language is selected? Can you also specify what languages were installed as part of the initial install of TIA Portal, and whether German was included? In other cases, this error could be solved as follows -> To try to solve the problem, delete the contents of the memory card in the CPU and re-download the project without making any other changes to the project. Can you try to see if this fixes the problem? Best regards!
|
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 11/29/2024 10:20 AM | |
|
Joined: 7/19/2022 Last visit: 1/14/2026 Posts: 436 Rating:
|
Hello Sc9667, Check that in the "Languages & resources > Project languages and Project texts" section you have enabled all the languages that you had in the old loaded project. Then, perform a complete compilation of both HW and SW and download the program into the PLC. |
|
If this Information really helps, you could use the Rate function |
|
| 12/3/2024 1:34 AM | |
|
Joined: 11/3/2022 Last visit: 5/2/2025 Posts: 5 Rating:
|
Hi Sir , I got the this setting when I got this program. I not sure what is initial setting. |
Follow us on