(0)| 12/4/2024 2:53 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi In principle, the procedure to install the software you specify should be to first install the base software of all the programs without any updates and then once you have everything installed, start with the upgrades. All these base software can be downloaded from SIOS: "SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V19 TRIAL Download", "SIMATIC WinCC Unified PC Runtime V19 Simulation & Trial" And then install the updates. I understand that when you say you have the Windows 24H2 version, you are referring to the Windows 11 version. The compatibility list is not yet in the Siemens 'Compatibility tool', although in principle they should be compatible.
|
|
If this Information really helps, you could use the Rate function |
|
Follow us on