1/8/2025 11:57 AM | |
Joined: 10/30/2018 Last visit: 9/12/2025 Posts: 24 Rating:
|
Hi Towome, By which HW configuration I can assign these values ('subnet', 'rack', 'sm', 'im', 'fm') to system attribute (S7_hardware). Programming Instructions, Creating Blocks for PCS 7 Thank you, Avinash
|
1/8/2025 5:13 PM | |
Joined: 9/21/2012 Last visit: 9/10/2025 Posts: 4708 Rating:
|
Subnet = Network, it can be MPI, Profibus or Profinet for example Rack = PLC rack SM = Signal module (I/O like input, output, analog...) FM = Function Module (Counter module or positioning module for example) IM = Interface Module |
Last edited by: Hati at: 01/08/2025 20:31:08Last edited by: Hati at: 01/08/2025 20:31:49 |
|
This contribution was helpful to
1 thankful Users |
1/9/2025 4:30 AM | |
Joined: 10/30/2018 Last visit: 9/12/2025 Posts: 24 Rating:
|
Thank you Towome, Let me brief what I understood if a device is connected behind Profibus/Profinet network then I can consider that one as a 'im', right? And can you provide the manual reference ?
|
Follow us on